Technical FAQs

Ask a Question

Can the A option be field installed to a standard ATV31...N4 unit?

No.   The A option, which includes the potentiometer and RUN/STOP buttons, is an integral feature to a drive unit and the option cannot be field installed.
For a drive with a control potentiometer and RUN/STOP buttons, add an ``A`` at the end of the catalog number when placing the order. For example, ATV31H037N4A.

Reviewed 6/2011

CTA-ID : 2017295
Was this helpful?
What can we do to improve the information ?