Technical FAQs

Ask a Question

What is Wattage Dissipated by the ATV58HC13N4XZU for calculating heat load when mounting in an enclosure?

2750 Watts at rated load in variable torque application.
1650 Watts at rated load in constant torque application.

Reviewed 12/2011

CTA-ID : 2017240
Was this helpful?
What can we do to improve the information ?