Technical FAQs

Ask a Question

What is the part number for the neutral assembly used on 42 or 54 ckt, 400A and 600A NQOD panels?

Standard aluminum = 80110-808-50

Copper base w/ aluminum branch terminations = 80110-808-52

Copper base w/ copper branch terminations = 80110-415-50

Available terminations are:

Aluminum main lug: (1) #1/0 - 750MCM or (2) #1/0 - 300MCM
Copper main lug: (1) #2 - 600MCM

Branch:

(3) #4 - 300MCM
(2) #14 - 2/0
(37) #4 - 14

Revised 4/27/04



CTA-ID : 10082
Was this helpful?
What can we do to improve the information ?