Technical FAQs

Ask a Question

What does the ending ``3`` represent in the catalog number of the GV2ME__3 starter?<br />

The digit ``3`` at the end of the catalog number is used to specify spring terminal connections on all the terminals.


CTA-ID : 2017780
Was this helpful?
What can we do to improve the information ?