Technical FAQs

Ask a Question

What are the repair parts for the HU661AWK, series F6? (may be shown as F06)

The repair parts for the HU661AWK, series F6 (F06) are as follows. No other parts are available. (NOTE: Descriptions below of ``left side`` and ``right side`` mean your left or right as you face the switch.)

-Line Base - one each of 4056792750 (left side base), 4056792650 (right side base), and 4056702801 (plastic connecting cam) (NOTE: arc suppressor not included)
-Line Base mounting screw - 4020515101 (6 total required, 3 for each line base)
-Arc Suppressor Assembly - 4056635550 (requires 1 for left side, and 1 for right side)
-Arc Suppressor mounting screw - 4020514501 (1 required per arc suppressor)
-Lug Assembly - 4025101652 (per lug)
-Lug Mounting Screw - 4020514202 (per lug)
-Mechanism Assembly - 4056646950 (also requires Switch Mechanism Gasket 4056603201)
-Handle - 4056663550 (requires Handle Gasket 4056603101)
-Lockplate - 4056672101
-Lockplate mounting screw - 2299940562 (2 required)
-Ground Lug - 4025101851 - (2 total required)
-Ground Lug Mounting Screw - 4020514801 (1 required)



CTA-ID : 2017870
Was this helpful?
What can we do to improve the information ?