Technical FAQs

Ask a Question

What is a 9007BY128?

That is a low temperature limit switch head. The Y form changes the temperature rating of the switch to -40 F to 185 degrees F.


CTA-ID : 2017693
Was this helpful?
What can we do to improve the information ?