Technical FAQs

Ask a Question

How many program configurations can be stored in the ATV31 Remote Keypad, VW3A31101?

Up to four complete configurations can be stored in the remote keypad display and transferred to other drive controllers of the same rating.
Four different operations for the same device can also be stored on the terminal.

Reviewed 7/2011


CTA-ID : 2017214
Was this helpful?
What can we do to improve the information ?