Technical FAQs

Ask a Question

What are the acceptable wire sizes for 8903SP lighting contactors?

Issue:
What are the acceptable wire sizes for 8903SP lighting contactors?

Product Line:
NEMA Lighting Contactors

Environment:
Products sold and used in the United States

Cause:
What are the acceptable wire sizes for 8903SP lighting contactors?

Resolution:
#14 - #2 copper or aluminum for power wires and #16 - #12 copper for control wiring.


CTA-ID : 2018076
Was this helpful?
What can we do to improve the information ?