Technical FAQs

Ask a Question

How do I select a 1200A HVL/cc duplex main in the product selector?

Issue:
How do I select a 1200A HVL/cc duplex main in the product selector?

Product Line:
HVLcc.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
Duplex bus has not been designed for the 1200A HVL/cc switch. There could be a heating issue for this application. No testing has been done on this. Also no bottom cross bus was designed for two 1200A HVL/cc mains adjacent to each other. The best way to enter this requirement in the product selector is all the mains feeders or to separate the mains by a feeder.


CTA-ID : 2018069
Was this helpful?
What can we do to improve the information ?