Technical FAQs

Ask a Question

How can the ATS48 unit be set up to operate with the correct line voltage?

There is nothing that needs to be set up because the power circuit adapts automatically to the input line voltage over a range of 208 to 690 VAC, +10%, -15%, 50 or 60 Hz.

CTA-ID : 2017150
Was this helpful?
What can we do to improve the information ?