Technical FAQs

Ask a Question

The customer has asked if it is possible to convert the SE frame breakers to electrically operated from manually operated.

Unfortunately it is not possible to convert a manually operated SE to an electrically operated. The mechanisms are different, and conversion is impossible.

CTA-ID : 2017147
Was this helpful?
What can we do to improve the information ?