Technical FAQs

Ask a Question

A 4054508701 crosses to a 4020284450K. A 40545008801 crosses to a 4054541301 which is then crossed to a 4020284450K. Are the 4054508701 & 40545008801 the same thing?

No, The 4020284450K is a kit that contains both the 4054508701 & 40545008801.


CTA-ID : 2017348
Was this helpful?
What can we do to improve the information ?