Technical FAQs

Ask a Question

What is the number for the floor operated attachment for the PINQO plug-in unit? <br /><br />What is the number for the floor operated attachment for the PIN100FA plug-in unit?

PI1QO for the PINQO and PINQOR
PI1FA for the PIN100FA

Not compatible with PowerBus225, the 100A rated busway.


CTA-ID : 2017343
Was this helpful?
What can we do to improve the information ?