Technical FAQs

Ask a Question

What are the termination data for QOU 10 - 60A circuit breakers?

The terminal lug wire size is (1) #14 - #2 AWG Cu or Al.


CTA-ID : 2017338
Was this helpful?
What can we do to improve the information ?