Technical FAQs

Ask a Question

Can NF be used at 380/220 50 hz ?

The NF panels can be used at 380/220 50 Hz. This can be selected under the International Voltages in Product Selectors.



Revised 4/5/04


CTA-ID : 2017038
Was this helpful?
What can we do to improve the information ?