Technical FAQs

Ask a Question

What is the deadfront part number provided in the N600SFB2KC or N600SFBKC sub-feed breaker kit?

Issue:
What is the deadfront part number provided in the N600SFB2KC or N600SFBKC subfeed breaker kit?

Produce Line:
NF panelboards and accessories sold and supported in the USA.

Environment:
Maintenance/repair

Cause:
Replacement deadfront part number

Resolution:
The N600SFB2KC and N600SFBKC subfeed breaker kits are now obsolete with no replacement. 







CTA-ID : 2016904
Was this helpful?
What can we do to improve the information ?