Technical FAQs

Ask a Question

What is the difference between the EK1020-1 and EK1020-2?

EK1020-1 is one normally open contact and one normally closed contact and the EK1020-2 is 2 normally open and 2 normally closed contacts.

CTA-ID : 2017288
Was this helpful?
What can we do to improve the information ?