Technical FAQs

Ask a Question

What are the replacement lugs for a PQ3606G Busplug

Request load base assembly 45201-624-50 which contains the lugs, base, and load side fuse clips for all three phases.This applies to Series 4 plug-in units only.

CTA-ID : 2017124
Was this helpful?
What can we do to improve the information ?