Technical FAQs

Ask a Question

What is a 25410-00084 that is supposed to be used with the ATV58 N2 Metasys Card Part number VW3A58345U?

25410-00084 is the Square D part number for their 9 Pin Male D-shell cable connector that may be used when an end of line termination is not needed.
This is a Phoenix contact connector  part number SUBCON-PLUS-M2 27 61 83 9.
If an end of the line termination is needed the Phoenix contact part number 27 61 50 9 along with a 120 ohm resistor and .001uF capacitor should be used.  
See page 17 of the VVDED300028NA R5/02 manual for further details.

CTA-ID : 2006507
Was this helpful?
What can we do to improve the information ?