Technical FAQs

Ask a Question

Is the main difference between panel mount and bus mount the fact that the panel mount version has line and load lugs?

There are two main differences. The panel mount version comes with a set of line and load lugs and includes a bus plate which makes its dimensions considerably different from the bus mount version.

CTA-ID : 15625
Was this helpful?
What can we do to improve the information ?