Technical FAQs

Ask a Question

Can a 3 pole 50 amp breaker be installed in an EZMR333225 using an adapter kit EZM125QOA?

No, a 70 amp QB QD QG or QJ is the low current rating available in the EZMR333225. The EZM125QOA is for use on single phase out sections only.


CTA-ID : 2017025
Was this helpful?
What can we do to improve the information ?