Technical FAQs

Ask a Question

Can you store and recall configurations on the ATV58 keypad?

Yes.

You can store up to four drive configurations, which can be read or downloaded to multiple drive controllers of the same horsepower and firmware revision.
Refer to page 91 on the keypad manual ( VVDED397047USR6/03) for instructions on storing and recalling paramaters.


CTA-ID : 2017281
Was this helpful?
What can we do to improve the information ?