Technical FAQs

Ask a Question

What are the repair parts for an EZM3400FSU, Series M01 main fusible switch unit?

Repair parts

Product Line:
EZM Metering

Repair parts

Only the parts listed below are considered field replaceable:
Customer Cover (top compartment) - EZM3400FSUTC
Molded Case Switch Cover (plastic) - BCM
Utility Cover (bottom pull box compartment) - EZM3400FSUBC
Cover Screws - 4020513002K
Molded Case Switch - LHF36000M
Fuses required (order separately) - Class T (300 Vac) 400A max.
Keps Nuts (1/2``-13 nut) - 2342702800
Bonding Strap - 7329696752
Mounting Channel - 7329654303
End Closing Cap Kit - EZMCAP
End Closing Cap Kit (Right Side Only Shallow) - EZMSCAP

CTA-ID : 2029914
Was this helpful?
What can we do to improve the information ?