Technical FAQs

Ask a Question

What is the difference between a SGA8189 and SGA8057?

The SGA8189 has a Brass housing that is no longer available, the SGA8057 has an Aluminum housing . There is a plastic housing SGA8072. Refer to D170 pg 15-74, and note that the DC ratings are different.

CTA-ID : 2029909
Was this helpful?
What can we do to improve the information ?