Technical FAQs

Ask a Question

What are the deadfront part numbers for an NF430L2 or NF430L2C interior?

Issue:
What are the deadfront part numbers for an NF430L2 or NF430L2C interiors?

Product Line:
NF Panelboards and Accessories

Environment:
Maintenance

Cause:
Replacement/repair

Resolution:
Order kit NFRPL430L2. This includes the MLO cover, the branch section cover, and the load end cover, as well as mounting hardware.


Note:  The 80113-171-50 (MLO cover) and 80113-175-50 (Load End cover) were previously available as separate items. These part numbers are now obsolete. Order complete kit NFRPL430L2 to obtain these parts.
Was this helpful?
What can we do to improve the information ?