Technical FAQs

Ask a Question

Can a shunt trip accessory be installed on medium voltage open or enclosed HVL switches?

Issue:
Can a shunt trip accessory be installed on medium voltage open or enclosed HVL switches?

Product Line:
HVL.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
The shunt trip switch requires a totally different operating mechanism than the standard HVL switch. This cannot be added on to an existing switch.
The stored energy mechanism (SEM) has separate opening and closing springs which are pre-charged and set on latches.


CTA-ID : 2017275
Was this helpful?
What can we do to improve the information ?