Technical FAQs

Ask a Question

Does Schneider Electric offer the Horizontal Ganged Metering suitable for use on 208Y/120Vac, three phase 4 wire?

Issue:
Product Design Features

Product Line:
Horizontal Gang Metering

Cause:
Application

Resolution:
No, the horizontal meters are ONLY available in single phase

 
Was this helpful?
What can we do to improve the information ?