Technical FAQs

Ask a Question

What are the dimensions of the RE9 timers?

0.89 inches (22.5 mm) wide, 3.07 inches (78 mm) tall, and 3.15 inches (80 mm) deep.


CTA-ID : 2017268
Was this helpful?
What can we do to improve the information ?