Technical FAQs

Ask a Question

Does the SC3040M200S accept tandem or Quad tandem branch breakers?

Issue:
Product Design Features

Product Line:
Combination Service Entrance Devices

Environment:
Branch breakers

Cause:
Accepting Tandem breakers

Resolution:
Yes, The SC3040M200S contains a 30space-40circuit load center that will accept up to 10 HOMT tandem breakers or 4 HOMT Quad tandem breakers.


CTA-ID : 2035252
Was this helpful?
What can we do to improve the information ?