Technical FAQs

Ask a Question

Can an 8501XDO be converted to AC control or an 8501XO be converted to DC control?<br /><br />

No. The AC and DC controlled devices are not the same size. The DC controlled devices are larger, because the coil is larger.


CTA-ID : 2017032
Was this helpful?
What can we do to improve the information ?