Technical FAQs

Ask a Question

Does the LUFP9 Devicenet option used with the drive require external 24v power supply?

Yes.
This componant is a gateway that bridges Modbus from the drive to convert to Devicenet protocol. The gateway does reqire 24 VDC +/- 10% to operate. Maximum power consumption is 280 mA.
It is not recommended to use the +24 from the drive to power the device.


CTA-ID : 2016864
Was this helpful?
What can we do to improve the information ?