Technical FAQs

Ask a Question

What contact block is used on a 9001K15?

Issue:
What contact block is used on a 9001K15

Product Line:
30mm Push Button

Environment:
9001K/SK/KX 30mm Push Buttons             

Cause:
Determine which contact block to use with application.                   

Resolution:                                                                 
Any 9001KA** type will work with this break-glass operator.
Was this helpful?
What can we do to improve the information ?