Technical FAQs

Ask a Question

Does the 9001 KR9R include a nameplate?<br />

Yes, the 9001 KR9R includes a nameplate marked ``PULL TO START-PUSH TO STOP``. Replacement nameplate is 9001 KN379.


CTA-ID : 2023504
Was this helpful?
What can we do to improve the information ?