Technical FAQs

Ask a Question

What kind of tool is required to remove the lugs from an LA breaker?

To remove the wire binding screw use a 3/8 hex wrench The tool to remove the lugs from the breaker is a Torx size 40.


CTA-ID : 2017018
Was this helpful?
What can we do to improve the information ?