Technical FAQs

Ask a Question

What is the contact orientation of the 9034LLV50 float level control switch?

When the float is mounted on the vertical shaft with the dimple below the midline (equator), the contact will be open when the float is up, closed when the float is down. When the dimple is above the midline, the contact will be closed when the float is up, open when the float is down.


CTA-ID : 2017016
Was this helpful?
What can we do to improve the information ?