Technical FAQs

Ask a Question

What is the scaling for the analog output for the ATV58 when set for motor current?

When configured for motor current (OCr), the analog output provides
a signal proportional to motor current. The minimum configured value
corresponds to zero while the maximum configured value of the
analog output corresponds to 200% of the drive controller constant
torque rating.

CTA-ID : 2016846
Was this helpful?
What can we do to improve the information ?