Technical FAQs

Ask a Question

Can the XB4BS9445 Key Release operator be depressed without the key installed?

Issue:
Can the XB4BS9445 Key Release operator be depressed without the key installed?

Product Line:
ZB4 and ZB5 Push Buttons

Environment:
ZB4 and ZB5 Emergency Stop Operators Push Buttons

Cause:
To clarify that the key does not need to be in device for button to be depressed

Resolution:
Yes, the key is inserted only to release the mushroom operator.
 
Was this helpful?
What can we do to improve the information ?