Technical FAQs

Ask a Question

What is the accuracy of the KWH or MWH power meter for the ATV58 type drives?

The kW and kWH measurements have +/- 5% accuracy.
The drive calculates the kW and kWH rather than making actual power measurements to the motor.
Information provided by the PLE (Product Line Engineer), Chuck Cudlipp.

CTA-ID : 2016664
Was this helpful?
What can we do to improve the information ?