Technical FAQs

Ask a Question

What is the measurement range of the motor power measurement for the ATV58 type drives?

The OPr display on the drive keypad is displayed as a percentage. It is the output power estimated by the drive controller.
100% corresponds to nominal power based on the rating of the drive.

With the analog output configured for motor power, OPR, the analog output provides a signal proportional to power drawn by the motor. The minimum configured value, AOL, corresponds to 0% of the nominal motor power, while the maximum configured value, AOH, corresponds to 200% of the nominal motor power.


CTA-ID : 2017082
Was this helpful?
What can we do to improve the information ?