Technical FAQs

Ask a Question

What are the part numbers of the terminal chamber cover plates (2 pieces, one large, one small) for the 13A enclosure?

Small cover: 39002-347-01 (rear cover with KOs)
Large cover: 39002-348-01 (front cover)
No hardware included with either cover


CTA-ID : 2016994
Was this helpful?
What can we do to improve the information ?