Technical FAQs

Ask a Question

What is the correct way to install the 31158-297-50 on the ATV58 drive?

Installation instructions are given in detail in the Instruction Bulletin 30072-450-45

Please disconnect power and check DC bus voltage before installing the kit.

This 9 pin 0-10 volt converter card is plugged into the 9 or 10 pin control terminal strip of the control board.
If the drive has a 10 pin connector make sure the 1st pin on the right side does match with the 24 volt pin on the drive. This will leave the analog output AO1 disconnected. This connection is not required for the Converter Kit. It may still be used if the application requires it.


CTA-ID : 2016693
Was this helpful?
What can we do to improve the information ?