Technical FAQs

Ask a Question

Does the ATV58 run time hours (rtH) start counting when drive is powered up or when motor is running?

The counter starts counting only when the motor is running (motor powered).


CTA-ID : 2016991
Was this helpful?
What can we do to improve the information ?