Technical FAQs

Ask a Question

What is the part number for the neutral assembly used on 225A NQOD panels w/ 30 ckts?

Standard aluminum = 80110-201-75

Copper base w/ aluminum branch terminations = 80110-201-77

Copper base w/ copper branch terminations = 80110-201-76

Available terminations are:

Al main lug: (1) #6 - 300MCM
Cu main lug: (1) #6 - 250MCM

Branch:

(32) #4 -14


Revised 4/27/04



CTA-ID : 2017529
Was this helpful?
What can we do to improve the information ?