Technical FAQs

Ask a Question

What is the part number for the neutral assembly used on 100A NQOD panels w/ 12, 18, 20, 24 or 30 ckts?

Standard aluminum = 80110-201-75

Copper base w/ aluminum branch terminations = 80110-201-77

Copper base w/ copper branch terminations = 80110-201-76

Available terminations are:

Al main lug: (1) #6 - 2/0
Cu main lug: (1) #6-250MCM

Branch:

(32) #4 - 14



Revised 4/27/04



CTA-ID : 2017528
Was this helpful?
What can we do to improve the information ?