Technical FAQs

Ask a Question

CU12L400CB Does Square d offer a 400/2 Main Breaker?

No - the CU12L400CB can accommodate 2-200/2 Main Breakers QDL,QGL or QJL Frame Breakers and 4-QOH Breakers up to 125/2.


CTA-ID : 2017527
Was this helpful?
What can we do to improve the information ?