Technical FAQs

Ask a Question

What is the part number for the replacement ground stab for the PQ4610G Bus Plug?

Only for Series 4 devices - see the nameplate to verify that you have a Series 4 device.
ground finger is 45201-554-01 (1 ea)
ground lug is 45118-056-50 (1 ea)
screw is 2142217161 (1 ea)
These parts will work with any 30, 60, 100 amp PQ Bus Plug (Ser 4).


CTA-ID : 2017254
Was this helpful?
What can we do to improve the information ?