Technical FAQs

Ask a Question

Are replacement parts and auxiliary accessories still available for the Class 8547, Class 8549, Class 8606, Class 8630, and Class 8640 pre-type S reduced voltage starters?

Class 9999 Type R6 & R7 disconnect switch and circuit breaker electrical interlooks are still available.

Type A, AF, AR, AU, B, C, CC, DD & FB thermal units are utilized with the Type S devices and are still available.

Some 31012-400-** (Type A Series B size 00 only) and 1861-S1-****(Type B All Series size 0) control coils may and still be available as they are also used with some active timing relay devices.
** & **** represent ending digets depending upon voltage required.

All other component parts, parts kits, coils, accessories, etc. are obsolete and no longer available.

If complete replacement device is required or desired, please use the Competitive Cross Reference tool link below.

CTA-ID : 2017076
Was this helpful?
What can we do to improve the information ?