Technical FAQs

Ask a Question

What is the wire range for the phase and neutral lugs on a QO2125BNF circuit breaker enclosure?

The phase and neutral lugs will accept a #14 - 2/0 AWG copper or #12 - 2/0 AWG aluminum conductor.


CTA-ID : 2035224
Was this helpful?
What can we do to improve the information ?