Technical FAQs

Ask a Question

Do we offer modification or a part # For the 8839 Enclosed ATV58 drives that would include the RFI filter?

There is not a standard Square D part number for RFI filters.
Radio Frequency Interference is not typically an issue when a drive is installed in a metal enclosure that is properly grounded. The metal enclosure acts as a Faraday shield. When power cables and control cables are correctly installed in separate conduits there is reduced trouble with RFI.
Ferrite cores can be installed around signal wires to reduce signal noise where necessary.

CTA-ID : 2016594
Was this helpful?
What can we do to improve the information ?