Technical FAQs

Ask a Question

Is there a lug kit for unit mount Powerpact PG, PJ, PK, or PL circuit breakers for use with (3) 600 kcmil cables?

A lug for (3) 600 kcmil wires is available for unit-mounted P frame breakers only. It will accept Al/Cu conductor sizes 350 to 600 kcmil. NOTE: It will not work with I-Line.
The kit numbers are:
AL1200P6KU (3 lugs per kit)
AL1200P6TKU (3 lugs per kit, control-wire tapped)
AL1200P6KU4 (4 lugs per kit)
AL1200P6TKU4 (4 lugs per kit, control-wire tapped)

CTA-ID : 2017390
Was this helpful?
What can we do to improve the information ?